Toolbar in the Automatic Diagnostic Event Summary
The following table describes the actions that can be accomplished using the Automatic Diagnostic Event Summary toolbar.
Icon | Action |
---|---|
![]() | Suppress selected event with comment. |
![]() | Unsuppress selected event with comment. |
![]() | Refresh the event queue and update the event list. |
![]() | Print event information. |
![]() | Select a configured filter. |
![]() | Remove the current filter. |
![]() | Edit filters. |
![]() | Find events using text strings. |
![]() | Configure sorting. |
Provide Feedback