Status bar in the Automatic Diagnostic Event Summary
The status bar at the bottom of the Automatic Diagnostic Event Summary gives an overview of the status of the alarm and event servers in the subscribed-to areas. For the connection status indicators, pointing to the icon will display a tooltip that lists the server names included in the subscribed-to areas and their connection status.
The following table describes the status indicator icons.
Icon | Description |
---|---|
![]() | The connection to all alarm and event servers is good. |
![]() | The connection to one or more event servers has been lost. |
![]() | The number of events in the event list. |
![]() | The number of Active and Unsuppressed events. When the count is zero, the icon is gray. |
![]() | The number of Active and Suppressed events. When the count is zero, the icon is gray. |
![]() | The number of Inactive and Suppressed events. When the count is zero, the icon is gray. |
![]() | The name of the filter used to specify which events are displayed in the events list or the text No Filter when there is no filter selected. |
![]() | The sort order of events in the event list. |
Provide Feedback