Create a subscription (Banner)

Create a new event subscription to specify the subscription settings. The newly created subscription removes the default subscription, which includes all areas, priorities, and event sources.
Multiple subscriptions are combined together. The subscription criteria are combined using the logical AND operator. For example, checking only the
Priority: Urgent
, entering an area of
Packaging Line
, and then entering an event source of
[BoxStuffer]*
subscribes to Urgent alarms from the packaging line whose names begin with [BoxStuffer].
To create a new subscription
  1. Open FactoryTalk View Studio.
  2. Open the display that includes the Alarm and Event Banner object.
  3. Right-click the Alarm and Event Banner object, and then click
    Properties
    .
  4. Click the
    Event Subscriptions
    tab.
  5. Under the
    Event subscriptions
    list, click
    Add
    .
  6. Type a unique name for the new subscription.
  7. Configure the subscription based on
    Scopes
    .
    1. Under the
      Scopes
      list, leave the default scope or click
      Browse
      .
    2. In the
      Select Scope
      browser, specify the scope for the events to subscribe to.
    3. Click
      OK
      .
    TIP:
    The default scope is
    (Any Scope)
    , which is equivalent to selecting the top node in the
    Select Scope
    browser.
  8. Configure the subscription based on
    Event sources
    .
    1. Under the
      Event sources
      list, leave the default event source or click
      Browse
      .
    2. In the
      Alarm Source Browser
      , select the area that contains the alarms you want to monitor in the list on the left.
    3. Double-click the alarms in the list on the right to add them to the
      Selected alarm sources
      list.
    4. Click
      OK
      .
    5. Under the
      Event sources
      list, click
      Add
      and then type the area name.
      TIP:
      If you subscribe to specific alarms and you configured the
      Scopes
      list, verify that the
      Scopes
      list includes the areas that contains those alarms.
    6. Press
      Enter
      . You cannot subscribe to the same alarm more than once.
      TIP:
      To change the name of an alarm, click the alarm name, click
      Edit
      , type a new alarm name, and then press
      Enter
      .To remove an alarm, click the alarm name, and then click
      Remove
      .
  9. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal