FactoryTalk Alarms and Events object model
The
FactoryTalk Alarms and Events
object model allows you to programmatically work with the graphic objects on a display. Using Microsoft Visual Basic for Applications Integrated Design Environment (VBA IDE), you can write code that uses objects in the FactoryTalk Alarms and Events
object model to interact with other objects at runtime.
Provide Feedback