FactoryTalk Web Token Authorization settings
How do I open FactoryTalk Web Token Authorization?
- Log on to theFactoryTalkNetwork Directory orFactoryTalkLocal Directory.
- InFactoryTalk Administration ConsoleExplorer, expandSystem > Policies > System Policies.
- Right-clickWeb Token Authorization, and then selectProperties.
The following table shows the FactoryTalk Web Token Authorization settings.
Setting | Description |
---|---|
Client ID | Shows the unique client identifier issued for the client. The third-party product uses the client ID and client secret pairs to get the web token to access the FactoryTalk-enabled products. The client ID cannot not be modified. |
Client Secret | Shows the client secret issued for the client. The third-party product uses the client ID and client secret pairs to get the web token to access the FactoryTalk-enabled products. The client secret is hidden by default. The client secret cannot not be modified. |
Generate | Creates the client ID and client secret pair. |
Description | Allows the user to describe the client ID and client secret pair. |
Add | Adds client ID and client secret to the list. |
Edit | Allows the user to edit the description of a client ID and client secret pair. |
Stop Edit | Cancels the editing. It is only available when you are in the edit mode, but no changes happened. |
Update | Saves the description changes. It is only available when you are in the edit mode and changes happened. |
Remove | Deletes the client ID and client secret you selected from the list. |
Disable | Disables the client ID and client secret you selected. |
Enable | Enables the client ID and client secret you selected. |
Status | Shows the status of the client ID and client secret you selected.
|
Provide Feedback