Export Policies
How do I open Export Policies?
- OpenFactoryTalk Administration ConsoleorFactoryTalk View Studio.
- SelectTools>Export Policies.
Use
Export Policies
to create an XML file containing the current FactoryTalk Directory
policy settings.The exported policies are limited to the policies accessible by the logged-on user. If the logged-on user does not have Read, Execute, or List Children permissions for a policy or its parent folders, that policy is not exported.
Use an XML or text comparison tool to determine policy changes between exported policy files.
Prerequisites
- Obtain user permissions to export policies:
- In, selectFactoryTalk Administration ConsoleSystem>Policies>>FactoryTalk Administration ConsoleFeature Security>Configure Security.
- Obtain permissions for each policy to be exported:
- Common > Read
- Common > Execute
- Common > List Children
To export policies to XML
- From theToolsmenu, selectExport Policies.
- Enter or browse to the path for the XML file.
- SelectExport.
Provide Feedback