Syslog Destination Setup settings
How do I open FactoryTalk Diagnostic Configuration?
- Log on to theFactoryTalkNetwork Directory orFactoryTalkLocal Directory.
- InFactoryTalk Administration ConsoleExplorer, expandSystem > Policies > System Policies.
- Right-clickFactoryTalk Diagnostics, and then selectProperties.
- In the left pane of theFactoryTalk Diagnostic Configurationdialog, expandDiagnostic Setup, and then selectSyslog.
The following table shows the Syslog Destination Setup settings.
Syslog Collector or Relay
Setting | Description |
---|---|
Host | Specifies the IPv4 address, IPv6 address, or the fully qualified domain name
(FQDN) of the computer hosting the Syslog collector. |
Port | Specifies an available port. The port range is from 1 through 49151. The default port is 514. |
Protocol | Selects the communication protocol.
|
Enable framing characters | Determines if the message is octet counted or delimited by trailing characters. It is only available when TCP is selected. |
Trailing | Sets the trailing characters. Available options are as follows:
It is only applied when Enable framing characters is selected. |
Message Buffering
Setting | Description |
---|---|
Use x MB of storage to buffer | Configures the storage size to buffer messages when the configured Syslog Collector cannot communicate with the local computer. The default size is 100 MB. The value range is from 10 through 5000. Changing the buffer size will affect all computers, and reducing the size could potentially remove messages stored in the buffer. |
This equals x messages | Shows the number of messages that can be cached using the buffer size. The FactoryTalk system will automatically calculate the approximate number of messages. |
Message categories
Configure using the intersection of FactoryTalk Diagnostic Audience and Severity that FactoryTalk Diagnostic messages will be forwarded to the configured Syslog Collector.
Audience options
Audience | Description |
---|---|
Operator | Typically, this option is assigned to messages that confirm the success or failure of an action initiated by people who are operating or using the FactoryTalk product or service. |
Engineer | Typically, this option is assigned to messages useful to control system designers, application engineers, and administrators for testing and troubleshooting FactoryTalk products and services. |
Developer | Typically, this option is assigned to messages useful to systems software developers for testing and troubleshooting software components and subsystems. |
Secure | Reserved for messages which need to be protected and retained based on
specifications for storing electronic records, such as US FDA 21 CFR Part 11. |
Severity options
Severity | Description |
---|---|
Error | Typically, this option is assigned to the most serious kind of error message, triggered by significant problems. |
Warning | Typically, this option is assigned to messages triggered by problems that are not necessarily critical, but which may cause future problems. |
Information | Typically, this option is assigned to messages that document the essential purpose of the FactoryTalk product or service, and which supplement and add more detail to "Audit" messages. |
Audit | Typically, this option is assigned to messages that indicate user activities which
are essential to the technology or purpose of the product or service. Note that,
Audit messages with this severity are not generated if the audit policy called
"Audit changes to configuration and control system" is disabled. Use FactoryTalk
Administration Console to configure audit policies. |
Beginning with FactoryTalk Services Platform version 6.50.00, these messages with the Secure
audience and Audit severity can be routed to:
- FactoryTalk AssetCentre log
- An ODBC database
- A Syslog Collector
Mapping
Configure the mapping of FactoryTalk Diagnostic audience message category to Syslog Facility
Code. The available Syslog Facility Codes include User-level, Local0, Local1, Local2, Local3,
Local4, Local5, Local6, and Local7. Syslog collectors use the Facility Code and Severity to
calculate priority.
Provide Feedback