Live Data Policy Properties
How do I open Live Data Policy Properties?
- InFactoryTalk Administration ConsoleExplorer, expandSystem > Policies > System Policies.
- Right-clickLive Data Policyand selectProperties.
Use the
Policy Settings
tab of Live Data Policy Properties
to select a default communications protocol for a distributed FactoryTalk
system.This setting affects communications between client and server services and between the
FactoryTalk Directory
and servers on the network. This setting is considered a "default". If the FactoryTalk Live Data
service detects that some components on the network are not compatible with the selected policy setting, the service overrides the policy and uses whichever setting is most likely to ensure uninterrupted communications. For example, for third-party servers and RSLinx Classic
, FactoryTalk Live Data
does not attempt a TCP/IP connection and always uses DCOM.Change this setting only if necessary, such as if the system is experiencing communications problems and it is necessary to switch to DCOM for troubleshooting purposes. Thoroughly test communications before deploying this change to a running production system. Many factors affect communications, including firewalls, closed ports, and differences in network architectures and configurations.
IMPORTANT:
Changing this policy setting can have unexpected results. Do not change this setting in a running production system. For changes to take effect, shut down and restart all computers on the network.
Provide Feedback