Default communications protocol settings

In a
FactoryTalk
distributed system, the communications protocol affects communications between client and server services and between the
FactoryTalk Directory
and servers on the network. This setting is considered a "default" because if the
FactoryTalk Live Data
service detects that some components on the network are not compatible with the selected policy setting, the service overrides the policy and uses whichever setting is most likely to ensure uninterrupted communications. For example, for third-party servers and
RSLinx Classic
,
FactoryTalk Live Data
does not attempt a TCP/IP connection and always uses DCOM.
Use the
Policy Settings
tab of
Live Data Policy Properties
to set the default protocol from
TCP/IP
to
DCOM
or vice versa.
The
FactoryTalk Services Platform
installation process evaluates the services and components on the network and sets the communication protocol appropriately. For example, if upgrading from an earlier version of the
FactoryTalk
platform to
FactoryTalk Services Platform
2.10 (CPR 9) or later, the communications default is automatically set to DCOM. If installing
FactoryTalk Services Platform
2.10 or later for the first time on a computer, the communications default is automatically set to TCP/IP. Typically, changing the default setting is not necessary or advisable.
Default protocol setting
Description
TCP/IP
An open communications protocol that typically is more reliable and has better performance than the proprietary DCOM protocol.
  • Choose this option only if all or most of the clients and servers on the automation network are upgraded to use
    FactoryTalk Services Platform
    v. 2.10 (CPR 9) or later.
  • Do not choose this option if the automation network is using older versions of the
    FactoryTalk Automation Platform
    v.2.00 (CPR 7) or earlier or if the system includes many third-party
    OPC
    servers and devices.
When this setting is changed from
DCOM
to
TCP/IP
, an audit message is logged to
FactoryTalk Diagnostics
indicating that the value changed from
False
to
True
.
DCOM
A proprietary communications protocol owned and managed by
Microsoft
.
Choose this option if:
  • Most of the clients and servers on the automation network are using older versions of
    FactoryTalk Automation Platform
    (v. 2.00, CPR 7 or earlier)
  • The system includes third-party
    OPC
    servers and devices
When this setting is changed from
TCP/IP
to
DCOM
, an audit message is logged to
FactoryTalk Diagnostics
indicating that the value changed from
True
to
False
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal