Authorize a service to use FactoryTalk Badge Logon
Use FactoryTalk Badge Authorization to authorize services to use the
FactoryTalk
Badge Logon function.The service that requests access to use the
FactoryTalk
Badge Logon function must be trusted by Rockwell Automation
. Please be aware that selecting Badge Only
as the system Login method
allows access to the system without authenticating the native FactoryTalk user. The system grants access solely on the identity of the badge. To maintain a strong security posture, we recommend that it is required to provide passwords in addition to presenting the badge, that is to say, you must select Password and Badge
as the system Login method
. Please note that the Badge Only
system Login method
cannot be used with Windows-linked users.
TIP:
To configure the Badge Authorization policy, log on to
FactoryTalk
with an account that is a member of the FactoryTalk
Administrators group. To authorize a service to use the
FactoryTalk
Badge Logon- Log on to theFactoryTalknetwork directory orFactoryTalklocal directory.
- InFactoryTalk Administration ConsoleExplorer, expand theSystem>Policies>System Policiesfolders.
- Right-clickBadge Authorizationand selectProperties.TheBadge Authorizationpolicy controls access by monitoring each service that is requesting theFactoryTalkBadge Logon function.
- In, click Add to permit access to a service that is requesting theFactoryTalkBadge AuthorizationFactoryTalkBadge Logon function.
- ClickOK.
Provide Feedback