Set logical name permissions
Starting from version 12.00, RSLogix 5000 supports Logical Names. You can use Logical Names to configure permissions for users and user groups to perform specific tasks in RSLogix 5000 and Studio 5000 Logix Designer software.
TIP:
We recommend that you use Permission Sets to improve the efficiency of the FactoryTalk Directory cache synchronization in Studio 5000 Logix Designer version 28.00 or later.
RSLogix 5000 is known as Studio 5000 Logix Designer starting from version 21.00.
Set permissions on the logical name to control whether a user-computer pair can:
- See the logical name (Read)
- Modify the properties of the logical name (Write)
- Change the security settings of the logical name (Configure Security)
- Delete the logical name (Delete)
- Perform actions defined in a user action group
Prerequisites
Setting logical name permissions requires these security permissions:
- Common > Read
- Common > Configure Security
To set logical name permissions
- InFactoryTalk Administration ConsoleExplorer, expandSystem > Networks and Devices>Logical Names,right-click the logical name, and selectSecurity.
- InSecurity Settings, in thePermissionstab, either:
- Set permissions by user:
- SelectUser.
- InUsers and Computers, select a user and computer.
- InAction, expand the category that contains the action to secure, and select the action.
- Set permissions by action:
- SelectAction.
- InAction, expand the category that contains the action to secure, and select the action. If the list of actions is blank, add users and computers first.
- InUsers and Computers, select a user and computer.
- SelectAlloworDeny, or clear both. Clear bothAllowandDenyto makeAction Groupsor the individual action group inherit its security settings from a resource higher in the directory tree.
- (optional) To control access to the selected action by another user or group, selectAdd, and inSelect User and Computer,select the user or group, and computer or group to add, and selectOK.
- When finished configuring security for the logical name, selectOK.
Provide Feedback