Select User and Computer

How do I open Select User and Computer?
  1. In the
    FactoryTalk Administration Console
    Explorer, right-click an item and select
    Security
    .
  2. On the
    Permissions
    tab
    ,
    select
    Add
    .
-or-
  1. In the
    FactoryTalk Administration Console
    Explorer, expand
    System > Policies >Product Policies
    and open a
    Feature Security
    item.
  2. From the
    Feature Security Properties Policy Setting
    tab, select
    Configure Security
    .
  3. In
    Configure Securable Action
    , select
    Add
    .
Use
Select User and Computer
to pair a group of users, or an individual user, with a group of computers, or an individual computer. Then, specify security settings for the pair.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal