Remove a user-computer pair

How do I open Select User and Computer?
  1. In the
    FactoryTalk Administration Console
    Explorer, right-click an item and select
    Security
    .
  2. On the
    Permissions
    tab
    ,
    select
    Add
    .
-or-
  1. In the
    FactoryTalk Administration Console
    Explorer, expand
    System > Policies >Product Policies
    and open a
    Feature Security
    item.
  2. From the
    Feature Security Properties Policy Setting
    tab, select
    Configure Security
    .
  3. In
    Configure Securable Action
    , select
    Add
    .
Remove a user-computer pair when it is longer necessary to specify permissions on a resource for the pair.
Prerequisites
  • Obtain the appropriate permissions to specify security settings on the selected resource.
To remove a user-computer pair
  1. Navigate to
    Select User and Computer
    , select the filter criteria to show the list of the users and user groups, and computers or computer groups to delete.
  2. In the
    Users
    list, select the user account or user group account that belongs to the pair being deleted.
  3. In the
    Computers
    list, select a computer account or computer group account that belongs to the pair being deleted.
  4. Select
    Remove
    .
  5. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal