Reset a password
Users occasionally forget user account passwords. Membership in the
FactoryTalk Security
Administrators group or equivalent permissions is required to manually reset a FactoryTalk
user account password. If the user account is a Windows
-linked account, the password must be reset in Windows
.To reset a password
- InFactoryTalk Administration ConsoleExplorer, expandSystem>Users, right-click the user account, and selectProperties.
- InUser Properties, selectReset Password.
- InNewpassword, type a new password for the user account.TIP:The maximum password length is 64 characters. However, the dialog box only displays 35 characters. Characters not shown are still included in the password.
- InConfirm new password, type the same password typed in the previous step, and selectOK.TIP:To reset a password in both a network directory and a local directory, reset the password in each directory.
Provide Feedback