New FactoryTalk Temporary User

How do I open New
FactoryTalk
Temporary User?
  1. In
    Explorer
    , expand
    System
    >
    Users and Groups
    .
  2. Right-click
    Users
    , point to
    New
    > then select
    FactoryTalk
    Temporary User
    .
Use
New
FactoryTalk
Temporary User
to allow users to temporarily utilize the privileges of another user in a different group. Create a special temporary user account, define who is permitted to authorize the use of this account, and choose a challenge and response scheme for generating the password for the account.
The user requesting access and the user authorizing access must reside in the same
FactoryTalk Directory
. Both users must connect to the
FactoryTalk Directory
or use a cached directory. If using a cached directory, it must contain the temporary user account.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal