FactoryTalk Batch Services Properties dialog—Archived Events tab

In the
FactoryTalk Batch Services Properties
dialog, use the
Archived Events
tab to configure the event types that
FactoryTalk®
Archiver will archive.

Archived Events tab settings

The selected event types on the
Archived Events
tab identify what electronic batch record data
FactoryTalk
Archiver writes to a SQL table in the
BatchHistoryEx
database.
TIP: For detailed definitions of the event types, refer to the .
There are three groups of event types:
  • FactoryTalk Batch
    events
  • FactoryTalk Batch
    Material Manager
    events
    TIP: The
    FactoryTalk Batch Material Manager events
    area is only accessible if, from the
    General
    tab, you selected the
    Enable FactoryTalk Batch Material Manager
    option.
  • FactoryTalk
    e
    Procedure®
    events
    TIP: The
    FactoryTalk eProcedure events
    area is only accessible if, from the
    General
    tab, you selected the
    Enable FactoryTalk eProcedure
    option.
To configure the options that define
FactoryTalk
Archiver data collection, including the name of the SQL table, go to the FactoryTalk Batch Services Properties dialog—Batch Reporting tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal