FactoryTalk Batch Services Properties dialog—Advanced tab

In the
FactoryTalk Batch Services Properties
dialog, use the
Advanced
tab to configure
FactoryTalk® Batch
Server extended properties.

Advanced tab settings

Extended properties are not available to configure in the user interface. Only configure them when directed to do so by
Rockwell Automation®
technical support.
Each property exists as a pair of strings,
Name
and
Value
.
Extended properties
Setting
Description
Name
Shows the names of
FactoryTalk Batch
Server extended properties. Each name must be unique, and meet the following requirements:
  • Maximum length of 64 characters
  • Begin with a letter
  • Contain only letters, numbers, and underscores
Value
Shows the values of
FactoryTalk Batch
Server extended properties. This field has a maximum length of 1,024 characters.
Sample extended properties
Name
Value
CommandTimeOut
60
IllegalUserBatchID
BAD_BATCH_ID
LicenseServerTimeout
120
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal