Edit FactoryTalk Batch Server properties
Open the
FactoryTalk Batch Services Properties
dialog to change a FactoryTalk® Batch
Server's configuration.Prerequisites
Modifying a
FactoryTalk Batch
Server requires these permissions for the
application or area:- Common > Create Children
- Common > Write
- Common > Read
To edit
FactoryTalk Batch
Server properties:- OpenFactoryTalk Administration Consoleand sign in to theFactoryTalkNetwork Directory.
- InFactoryTalk Administration ConsoleExplorer, expand applications or areas until theFactoryTalk BatchServer is visible.
- Right-click theFactoryTalk BatchServer, and selectProperties.
Provide Feedback