Configure FactoryTalk Batch High Availability (HA)
Optionally, set up a secondary
FactoryTalk® Batch
Server to create a FactoryTalk Batch
Server pair that can resume or continue batch execution on
the other member of the pair.To set up a secondary
FactoryTalk Batch
Server:- In theFactoryTalk Batch Services Propertiesdialog, use theSecondary Servertab to configure secondaryFactoryTalk BatchServer options.
- In theFactoryTalk Batch Services Propertiesdialog, use theProject Settingstab to configure the project settings for a computer on which the secondaryFactoryTalk BatchServer is installed.
Provide Feedback