Device Properties

For control hardware displayed in the
Networks and Devices
tree, use
Device Properties
to:
Setting
Description
Device path
Displays the network relative path of the device. This setting is read-only.
Logical name
Associates a device with a logical name. Select a logical name to view the area associated with the logical name. The area indicates the resource grouping to which the logical name belongs. Do either:
  • To create a new logical name, select
    <New...>
    . In
    New Logical Name
    , enter a descriptive name and select
    OK
    .
  • To associate the device with an existing logical name, or to change the logical name associated with the device, under
    Logical name
    select the logical name.
  • To remove the logical name the device is associated with, select
    None
    . The security system automatically uses the security permissions associated with the device's network relative path.
Area associated with
If the selected logical name is a member of a hardware resource grouping, this setting displays the area from which the logical name inherits its security permissions. This setting is read-only.
Remove
To remove the logical name from the area, select
Remove
. This removes the logical name from the resource grouping.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal