Delete a logical name
Delete a logical name from
Networks and Devices
when not needed as an alias for a control device or network. After deleting a logical name, the security permissions for the devices associated with it revert to the permissions of the device or network.
IMPORTANT:
Because
RSLogix 5000
controllers do not use network relative paths, deleting a logical name associated with a RSLogix 5000
controller can cause unexpected results.To delete a logical name
- InFactoryTalk Administration ConsoleExplorer, expandNetworks and DevicesuntilLogical Namesis visible.
- Right-click the logical name and selectDelete.
Provide Feedback