Access checks do not work as expected

Action groups and resource groupings are not supported on
FactoryTalk Automation Platform
2.00 (CPR 7).
To use action groups or resource groupings, upgrade all computers participating in the Network Directory to
FactoryTalk Services Platform
2.10 (CPR 9) or later.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal