Initial Connection
How do I open Initial Connection?
Initial Connection
appears automatically after you launch FactoryTalk Live Data Test Client
. To use Initial Connection
to switch to a different data source, click File > Reconnect.
Use
Initial Connection
to:- Connect to an OPC DA server, such asRSLinx Classic
- Connect to aFactoryTalkserver, such asFactoryTalk LinxorFactoryTalk View SE
- Load a configuration file containing data items from anOPCorFactoryTalkserver
Configure the settings to establish the initial connection between the
FactoryTalk Live Data Test Client
and the data source.Setting | Description |
---|---|
OPC DA Server | Connect to an OPC DA server, such as RSLinx Classic, to monitor, read, and write data items in the data server. |
Factory Talk | Connect to a FactoryTalk server, such as FactoryTalk Linx or FactoryTalk View SE, to monitor, read, and write data items in the data server. |
Load Config File | Load a config file to open a collection of previously saved data items and groups for monitoring. A config file is saved in XML format. |
OPC DA Server Machine | If the OPC DA server is located on the same computer as the FactoryTalk Live Data Test Client, select Local. If the OPC DA server is located on a remote computer, select Remote, and then enter the name of the computer in the box. |
OPC DA Server Locale ID | The locale identifier for the OPC DA Server machine. |
Provide Feedback