Connect FactoryTalk Live Data Test Client to a FactoryTalk server

Connect
FactoryTalk Live Data Test Client
to a
FactoryTalk
server, such as
FactoryTalk Linx
, an OPC UA server connected to the FactoryTalk Linx OPC UA Connector, or
FactoryTalk View SE
, to monitor, read, and write data items in the data server.
Prerequisites
  • If connecting to a data server in a
    FactoryTalk
    Network Directory, configure the Network Directory Server location.
To connect to a
FactoryTalk
server
  1. Start the
    FactoryTalk
    server. For example:
    • To monitor tags in a
      FactoryTalk Linx
      server, start
      FactoryTalk Linx
      .
    • To monitor tags in a
      FactoryTalk View SE
      server, start the
      FactoryTalk View SE
      Client or
      FactoryTalk View Studio
      , and then open the application.
    • To monitor tags from a
      FactoryTalk Linx
      OPC
      UA Connector, start the connector and an OPC UA server it is configured to interface with.
  2. Go to
    Rockwell Software > FactoryTalk Tools
    and open
    FactoryTalk Live Data Test Client
    .
  3. In
    Initial Connection
    , select
    FactoryTalk
    .
  4. In
    Select
    FactoryTalk Directory
    , select the
    FactoryTalk Directory
    that contains the server.
  5. (optional) If prompted, log on to the
    FactoryTalk Directory
    .
  6. Expand the directory tree, then select the
    FactoryTalk
    server from the list of available servers, then select
    OK
    .
    If the
    FactoryTalk
    server is not shown, verify the correct
    FactoryTalk Directory
    selection, then verify it is running and accessible over the network.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal