Advanced

How do I open Advanced?
From the Data menu, choose
Add Item
to open the
Add Item
dialog box. Click the
Advanced
button.
TIP:
You cannot add a data item while HMI Emulation Mode is running.
Use
Advanced
to create an array of items to be added to a group.
IMPORTANT:
The array settings cannot be modified after they are created. To edit data items after you have added them in
Advanced
, edit each data item individually, or remove the data items from the group and then add them again in
Advanced
.
Setting
Description
Datatype
Select the data type for the values to monitor. If unsure of the data type, select
Native
.
Active
To display information about the data item (for example, changes to its status or value at the server), select the
Active
check box. To prevent information about the data item from being displayed in the
FactoryTalk Live Data Test Client
, clear the
Active
check box.
ItemID
Type the address of the data items to load, using the syntax (topic.data1[%d]).
Example: One-dimensional array
To load 100 data items at the N7: address of a
PLC-5
, type N7:%d. Specify the address range in the Min and Max boxes. To create a multi-dimensional array, add up to two more %d placeholders.
Example: Three-dimensional array
To load data from
FactoryTalk Linx
using a three-dimensional array of data items, type
TOPIC%d%d.DATA%d
. This might return data such as
TOPIC1000.DATA0
,
TOPIC1011.DATA1 . . . TOPIC20099.DATA80
.
Array Dimension
The number of array dimensions are selected automatically, depending on how many %d placeholders added in
ItemID
. Loading data items in more than 3 dimensions is not supported.
Min
Type the starting value for each dimension of the array. For example, in the three-dimensional array shown above, the starting values are 100, 0, and 0.
Max
Type the ending value for each dimension of the array. For example, in the three-dimensional array shown above, the ending values are 200, 99, and 80.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal