Change the group update rate
Change the group update rate to increase or decrease the rate at which all data items in the group are updated.
The rate at which the data server is updating the value of the data item is shown in the
Updates (/Sec)
column of the viewer. If the data server is sending data faster than the screen update rate, some changes to data items will not be displayed. If the data server is sending data slower than the screen update rate, the FactoryTalk Live Data Test Client
might be generating unnecessary traffic on the network.To change the group update rate
- InFactoryTalk Live Data Test ClientselectGroup>Group State.
- InUpdate Rate, type the number of milliseconds at whichFactoryTalk Live Data Test Clientupdates data items in the group, then selectOK.
Provide Feedback