Toolbox
Use
Toolbox
to find and add program elements to a language editor.Toolbox
contains the elements associated with the ladder diagram language, function block diagram language, or structured text language.In
Toolbox
:- UseSearchor select a category from the list to filter program elements.
- Hover over an element to view its name, description, and image.
- Drag the border between the category and list pane to resize the panes.
To | Do this |
|---|---|
Pin or unpin Toolbox | Do one of the following:
|
Shrink down Toolbox and leave just a tab | Select , and then select Collapse . |
Show the content of Toolbox | Select , and then select Expand . |
Hide Toolbox | Select , and then select Close . |
Provide Feedback
.
, and then select