Ladder editor Toolbox
Use the ladder editor
Toolbox
to add program elements to the ladder diagram.Toolbox
is displayed by default. If it is hidden, do one of the following:- From the pane bar, select
. - From theViewmenu, selectToolbox.
Ladder editor Toolbox

Item | Description |
|---|---|
![]() | Adds a rung to the ladder diagram. |
![]() | Contains the entered element name for quick finding.
As you enter, elements that contain the search text appear in Toolbox . |
![]() | Adds a branch to the ladder diagram. |
![]() | Adds a parallel branch to an existing branch. |
![]() | Displays the categories of the program elements. Selecting a category filters the displayed program elements. |
![]() | Displays the program elements of the selected category. |
Provide Feedback