Add a description
Descriptions are free-format text that can be inserted anywhere in the function block diagram (FBD) program. Descriptions are for documentation purposes only and are not acted upon by the program.
To add a description
- FromToolbox, drag
to the editor. - In the text box, enter the description.
Provide Feedback