Proportional Integral Derivative (PID) instruction
Use the Proportional-Integral-Derivative (PID) instructions to control the process more accurately using PID functionality.
Instruction | Description |
|---|---|
Configure and control the outputs that control physical properties such as temperature, pressure, liquid level, or flow rate using process loops. |
Provide Feedback