Process instructions
Use Process instructions to monitor and maintain process loops for quantities such as pressure, temperature, flow rate, and fluid level. Process instructions regulate the course by sending an output signal to the control valve.
Instruction | Description |
|---|---|
Performs a Boolean hysteresis on the difference of reals. | |
Configures and control the inputs and outputs used for the Proportional Integral Derivative (PID) logic. | |
Use the Proportional-Integral-Derivative (PID) instructions to control the process more accurately using PID functionality. |
Provide Feedback