RTC_READ (read real-time clock)
The RTC_READ instruction reads the real-time clock (RTC) module information.
Operation details:
- Micro810 or L20E controller with embedded RTC:
- RTCBatLow is always set to zero (0).
- RTCEnabled is always set to one (1).
- When the embedded RTC has lost its charge/memory due to loss of power:
- RTCData is set to 2000/1/1/0/0/0.
- RTCEnabled is set to one (1).
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the Micro810, L20E, L50E, and L70E controllers.
RTC_READ

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL | Instruction block enable.
|
RTCData | Output | RTC | RTC data information: yy/mm/dd, hh/mm/ss, week .RTCData output is defined using the RTC data type. |
RTCPresent | Output | BOOL |
|
RTCEnabled | Output | BOOL |
|
RTCBatLow | Output | BOOL |
|
ENO | Output | BOOL | Enable output. Applies only to ladder diagram programs. |
Parameter | Parameter Type | Description |
|---|---|---|
Year | UINT | The year setting for the RTC. 16-bit value, and the valid range is from 2000 (Jan 01, 00:00:00) through 2098 (Dec. 31, 23:59:59). |
Month | UINT | The month setting for the RTC. |
Day | UINT | The day setting for the RTC. |
Hour | UINT | The hour setting for the RTC. |
Minute | UINT | The minute setting for the RTC. |
Second | UINT | The second setting for the RTC. |
DayOfWeek | UINT | The day of the week setting for the RTC. This parameter is ignored for RTC_SET. |
RTC_READ examples
RTC_READ function block diagram example

RTC_READ ladder diagram example

RTC_READ structured text example

Provide Feedback