Date Time instructions
Use Date Time instructions to control operations based on time or configure the calendar and the clock.
Instruction | Description |
|---|---|
Turn on an output if the value of the real-time clock is in the range of the Year Time setting. | |
Reads the real-time clock (RTC) module information. | |
Sets RTC data to the RTC module information. | |
Computes the time difference between TimeA and TimeB. | |
Turns on an output if the value of the real-time clock is in the range of the Time of Week setting. |
Provide Feedback