AWA (ASCII write append)
The AWA instruction writes a string with two appended (user-configured) characters to an external device.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the L20E, L50E, and L70E controllers.
AWA

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
IN | Input | BOOL | Rung input state.
|
AWAInput | Input | AWAAWT | The channel and number (Length) of the characters to write to the buffer. The maximum is 82. Use the AWAAWT data type to define Channel, Length, and Cancel parameters for AWAInput. |
Q | Output | BOOL | Indicates when the write is ongoing or complete. Outputs of this instruction are updated asynchronously from the program scan. Output Q cannot be used to re-trigger the instruction because IN is edge triggered.
|
NumChar | Output | UINT | The number of characters. NumChar might be less than the Length requested to be transmitted if the length of the Source String is shorter than the requested Length. Updates when the transmission is complete and Q is TRUE. |
Error | Output | BOOL | Indicates the existence of an error condition.
|
ErrorID | Output | UINT | A unique numeric that identifies the error. The errors for this instruction are defined in ABL error codes. |
Error code | Error description |
|---|---|
03 | Transmission cannot be completed because the Clear-to-Send signal was lost. |
06 | Illegal parameter was detected. |
07 | Cannot complete ASCII send or receive because channel configuration has been shut down using the channel configuration dialog. |
08 | Cannot complete ASCII Write due to an ASCII transmission already in progress. |
09 | ASCII communication requested is not supported by current channel configuration. |
10 | The Cancel was set, stopping instruction execution. No action required. |
14 | The ACL function block was canceled. |
16 | Serial port is not supporting RTS or CTS control lines. |
AWA examples
AWA function block diagram example

AWA ladder diagram example

AWA structured text example

Provide Feedback