Convert pulses per revolution and velocity

In
FactoryTalk Design Workbench
, the
Micro800
controllers that support motion use high-speed pulse-train outputs (PTO) for axis positioning. The axis can be configured in revolutions per minute (rpm) or user-defined unit per second. The user-defined unit is specified using the
Position
parameter on the Axis - Motor and Load configuration page.
To convert from rpm (steps) to user-defined units, use the following formula:
Formula to convert from rpm (steps) to user-defined unites
Formula to convert from rpm (steps) to user-defined unites
To convert from velocity to user-defined units per second or to rpm, use the following formula:
Formula to convert from velocity to user-defined unites per second or rpm
Formula to convert from velocity to user-defined unites per second or rpm
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal