Axis - Limits configuration page
Configure the motion settings for the
Micro800
controllers that support motion. Add an axis to create the axis configuration pages.Use the
Axis<x> - Limits
configuration page to:- Specify the stop behavior of the axis: immediate stop or deceleration stop.
- Configure the hardware limits for the axis. TheHard Limitsparameters correspond to the input signals that are received from hardware devices, such as limit switches and proximity sensors. The hardware input signals detect the presence of the load at the maximum upper and minimum lower extents of available motion for the load or movable structure that carries the load, such as a load tray on a transfer shuttle. The hardware parameters are then mapped to discrete inputs that are associated with data tags and variables.
- Configure the software limits for the axis. TheSoft Limitsparameters correspond to the data values that are managed by the controller and are based on the user-defined stepper commands and the motor and load parameters that you specified on the Motor and Load configuration page.
Setting | Description |
|---|---|
Hard Limits | |
When hard limit is reached, apply | Specifies the stop behavior of the axis:
The options are:
|
Lower hard limit | Makes the lower hard limit parameters available or not available for configuration. The parameters are available by default.
|
Upper hard limit | Makes the upper hard limit parameters available or not available for configuration. The parameters are available by default. Active level specifies the active level of the input signal that is sent from a hardware device such as a switch. The default active level is Low .Switch input is read-only and it specifies the wiring information for a hardware device. |
Soft Limits | |
Lower soft limit | Makes the Lower soft limit parameter available or not available for configuration. It is not available by default.You can make either the Lower soft limit or the Upper soft limit parameter available individually.The value range is relative to the value that you specified for Pulses per revolution on the Motor and Load configuration page. The default value for Pulses per Revolution is 200.0 .The default range for the value of Lower soft limit is from –10732174 (–2146435072/200) through 10732174 (2146435072/200).The range for the available values is from –2146435072 through 2146435072 steps represented in single precision floating point format. The default value is 0.0 mm. |
Upper soft limit | Makes the Upper soft limit parameter available or not available for configuration. It is not available by default.The value range is relative to the value that you specified for Pulses per revolution on the Motor and Load configuration page. The Upper soft limit value must be greater than the Lower soft limit value.The default range of the Upper soft limit value is from –10732174 (–2146435072/200) through 10732174 (2146435072/200).The range for the available values is from –2146435072 through 2146435072 steps represented in single precision floating point format. The default value is 0.0 mm. |
emergency stop profile | Goes to the Dynamics configuration page, where you can specify the emergency stop profile parameters. |
Provide Feedback