LCD Module configuration page
The
LCD Module
configuration page is available for Micro810
controllers. Use the page to do the following actions:- Add an LCD module to theMicro810controller configuration.
- Back up user programs and function files to the LCD module.
- Restore user programs and function files from the LCD module to theMicro810controller configuration.
- Open theLCD variablesview to select which variables to monitor using the LCD module.
- View the connection status of the LCD module.
- Configure the hardware settings forpush button key read.
Setting | Description |
|---|---|
Attach LCD module | Determines whether to add the LCD module to the Micro810 controller project. By default, the LCD module is not part of the Micro810 controller project. |
Status | Indicates the status information of the LCD module and the controller.
Status includes the following read-only values:
|
Diagnose | Opens the controller diagnostics view. The Diagnose button is available when the controller is online. |
LCD variables | Opens the LCD variables view. The view is available when the following conditions are met:
You can select up to 200 variables to monitor using the LCD module's Main menu. Exceeding the limit will result in build problems. |
LCD Module Settings | |
Enable push button key read | Turns on the KEY_READ function block instructions that read the key status of the LCD module. By default, the KEY_READ function block instructions are turned off. |
Backlight mode | Specifies the backlight behavior for the remote LCD. Options are as follows:
Interval is the default selection. |
Time | Specifies the backlight interval when Backlight mode is set to Interval . The value is from 10 through 120 seconds. The default value is 30. |
Contrast | Specifies the backlight contrast on the LCD. The value is from 0 through 100 percent. The default value is 50 percent. |
Backup/Restore | |
Load on power up | Specifies LCD module behavior when turning on the controller. Options are as follows:
The default setting is Disabled . |
Back up to the LCD module | Starts backing up user programs and Micro810 controller project files to the LCD module. The Backup to the LCD module button is available when the following conditions are met:
|
Restore from the LCD module | Starts restoring user programs and Micro810 controller project files from the LCD module to the project.If the 2080-LCD hardware is secured with a password, the controller password must align with the 2080-LCD password. The Restore from the LCD module button is available when:
|
Provide Feedback