Motion axis monitoring
The
Axis monitor
page is available when:- The controller is online.
Use the
Axis monitor
page to:- Select the axis you want to monitor.
- View the axis state, velocity, movement, current position, and target position.
- View the error code and description if the axis encounters an error.
Item | Description |
|---|---|
Axis name | Specifies the names of axes assigned to the controller. Up to three axes are listed depending on the controller type and the number of axes configured. |
Axis state | Specifies the state of the axis that you are monitoring. Options are:
|
Axis homed | Specifies when the axis is in the home position. Values are:
|
Movement | Describes the movement for the axis. When an axis is not moving, it is Idle. Values are:
|
Error description | Displays the error code and description when an error occurs in the axis. It is empty when there are no errors.
For more information, see AxisErrorID error codes. |
Position and Velocity | |
Command position | Specifies the current position of the axis when the command is executing. |
Target position | Specifies the value of the target position defined for the axis.
Use the Position input value of the MC_MoveAbsolute function block to define the target position. |
Speed | Specifies the current velocity when the command is executing. |
Target velocity | Displays the target or maximum velocity for the axis.
Use the Velocity input value in the MC_MoveRelative, MC_MoveAbsolute, or MC_MoveVelocity function block to define the target velocity. |
Provide Feedback