Customize variable grid columns
Customize the variable grid to hide or show columns, adjust the column display order, or sort the variables in ascending or descending order.
TIP:
The
Name
column cannot be hidden, and its position as the first column from left to right cannot be changed.To customize variable grid columns
- Customize the variable grid columns.
- To show or hide a column, hover over a header cell, select
, select
, and then select or clear a column name checkbox. - To change the order of columns, drag the column to the position you want.
- To sort variables in ascending or descending order, in the header cell, select
or
. - To turn off sorting, select
or
multiple times until it becomes inactive.
Provide Feedback