Open the local variable grid
Local variables are the variables assigned to a specific program in the project and are available only to the program.
To open the local variable grid
- InProject Organizer, go to , and then under<program-name>, double-clickLocal Variables.
Provide Feedback