Pair a PTO axis and motion feedback axis
Pair an embedded PTO axis with a feedback axis to allow the feedback axis to:
- Use the paired PTO axis's settings.
- Serve as feedback for the existing paired PTO axis.
After you pair a PTO axis and a motion feedback axis, the settings for the motion feedback axis become read-only.
Prerequisites
- Add a 2080-MOT-HSC to the controller project.
- Configure an embedded PTO axis.
To pair a PTO axis and motion feedback axis
- InProject Organizer, go to .
- Open the2080-MOT-HSCpage by doing one of the following:
- Double-click2080-MOT-HSC.
- Select2080-MOT-HSC, and then select theEnterkey.
- On the 2080-MOT-HSC page, selectConfiguration.
- From theEnable plug-in withlist, selectFeedback axis.UnderConfiguration, theFeedback Axisnode is created.
- On the2080-MOT-HSCpage, selectFeedback Axis.
- On the FBAxis<x>- General configuration page, from thePair withlist, select an axis.
Provide Feedback