Device Level Ring (DLR)
Device Level Ring (DLR) is an EtherNet/IP™ protocol that is defined by ODVA. DLR provides a means to detect, manage, and recover from a single fault in a ring-based network.
A DLR network includes the following types of ring nodes.
Node | Description |
|---|---|
Ring supervisor | A ring supervisor provides these functions:
A DLR network requires at least one node to be configured as ring supervisor. By default, the supervisor function is disabled on supervisor-capable devices. |
Ring participants | Ring participants provide these functions:
When a fault occurs on the DLR network, ring participants reconfigure themselves and relearn the network topology. |
Redundant gateways (optional) | Redundant gateways are multiple switches that connect to a DLR network and also connect together through the rest of the network. Redundant gateways provide DLR network resiliency to the rest of the network. |
Depending on their firmware capabilities, both devices and switches can operate as supervisors or ring nodes on a DLR network. Only some devices, such as switches, can operate as redundant gateways.
For more information about DLR, see the EtherNet/IP Device Level Ring Application Technique, publication ENET-AT007.
Use DLR in a Redundancy System
For supported DLR I/O network topologies and design guidelines for high availability systems, see the High Availability Systems Reference Manual, HIGHAV-RM002.
Provide Feedback