Configure the EtherNet/IP Network

Before you begin to configure the communication modules in the redundant chassis pair, verify the following:
  • The redundancy modules are installed and connected in the redundant chassis.
  • The partner communication modules are able to communicate to each other over the Ethernet network.
  • You know the subnet mask and gateway address for the Ethernet network on which the redundant communication modules operate.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal