Configure a controller project

Before creating a new
Logix Designer
project, configure controller and security settings.
To configure a controller project
  1. In the
    Revision
    list, select a firmware revision for the controller. The latest revision of firmware is the default.
  2. In the
    Security Authority
    list, select a security option:
    • No Protection
      - All users can view and edit the project.
    • FactoryTalk Security
      - Only users authenticated through
      FactoryTalk Security
      can view and edit the project.
      1. (optional) Select Use only the selected Security Authority for authentication and authorization to associate this project with a specific Security Authority. When this check box is selected, users interacting with this project must be authenticated and authorized by the same Security Authority that was used to secure the project. Otherwise, unauthenticated users must rely on Guest User permissions.
        TIP:
        Guest User permissions are cached within the project. The
        Logix Designer
        application uses Guest User permissions when the project is opened but not connected to the
        FactoryTalk
        Security Authority that secures the project. By default, all Guest User permissions are denied. Guest User permissions are configured in the
        FactoryTalk Administration Console
        .
      1. Select
        Logical Name <Controller Name>
        or
        Permission Set
        to apply specific permissions to the controller.
        Select
        Logical Name <Controller Name>
        to apply
        a Logical Name in
        FactoryTalk Services Platform
        that has the same name as the controller. If there is no existing Logical Name that matches the controller name, a new Logical Name is created with the controller's name. The new Logical Name inherits permissions from its parent resource. See
        FactoryTalk
        Help for more information on how networks and devices inherit security permissions.
        Select
        Permission Set
        to apply a specific set of permissions to the controller. The permission sets in the list are maintained in
        FactoryTalk Services Platform
        and identify a set of actions that are allowed or denied for a particular user and computer combination.
  3. (optional) In the
    Description
    box, enter a description for the controller.
    TIP:
    The description is limited to 128 bytes. Standard ASCII characters consume 1 byte per character, allowing for 128 characters. Characters in some languages require up to three bytes per character, resulting in less than 128 characters.
  4. Select
    Finish
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal