Edit a substitution
Edit a substitution to change the scope or replacement conditions when needed.
To edit a substitution
- In the decorator pane, click the Substitutions tab, either:
- Double-click the substitution.
- Right-click the substitution, then selectEdit.TheSubstitution Builderwindow opens.
- Edit the substitution as needed.
- ClickOKto save the edits to the substitution.
Provide Feedback