Add parameter links

Parameter links are used to read or write the parameter values between a library object and linked library object. Parameter links display the direction of the flow of information.
To add parameter links
  1. In the decorator pane, click the
    Linked Libraries
    tab.
  2. Click the linked library in which to add the parameter links. The
    Add new parameter link
    button in the
    Parameter Links
    toolbar becomes active.
  3. In the
    Parameter Links
    pane, either:
    • Click the
      Add new parameter link
      button.
    • Right-click an empty row and click
      Add
      .
      The Parameters browser window opens.
  4. Select a parameter and click
    OK
    .
    The new parameter will appear in the
    Parameter Links
    pane.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal