Parameters browser
How do I open the Parameters browser window?
- In the decorator pane, click theLinked Librariestab.
- Click the linked library in which to add the parameter links. TheAdd new parameter linkbutton in theParameter Linkstoolbar becomes active.
- In theParameter Linkspane, either:
- Click theAdd new parameter linkbutton.
- Right-click an empty row and clickAdd.
Use the
Parameters browser
window to define the parameter links for a linked library.The
Parameters browser
window includes these items:Item | Desription |
|---|---|
Library Catalog Number | The library object name, which appears when the library object is registered in the Application Code Manager application. |
Library Location | Where the library is located. |
FindPartial/FindPrefix | Searches the library for parameters that include the text string typed in the adjacent box. Two methods of search are provided:
|
Parameter list | The parameters available in the library object. If a search string is specified, the parameters are limited to those that meet the search criteria. |
Provide Feedback