Add a linked library
A linked library is a library object containing elements that are shared with other libraries. Linked libraries specify the relationships between library objects. The links are applied as decoration to Logix code in place of parameters.
To add a linked library
- In the decorator panel, either:
- Click
on the Linked Librariestab toolbar. - In theLinked Librariestab, right-click in the top grid and then clickAdd New Link.The Add New / Edit Linked Library window opens. By default libraries resident in the ACD file are displayed in the list.
- InSelect the library you want to link to, click a library object. The object parameters are displayed in the right panel.TIP:If no libraries are displayed in the list, then it means that the ACD file only contains the one library.To link to libraries contained in the ACM database, clickConnect to Database.
- InLink Name, type a name and then pressEnter.
- Populate other fields as needed.
- ClickOK.The link appears in the list on theLinked Librariestab.
Provide Feedback