Add New / Edit Linked Library
How do I open Add New / Edit Linked Library?
- In theLibrary Objectscolumn, select a library.
- In the decorator panel, select theLinked Librariestab.
- Right-click in the top list of linked libraries, then selectAdd New Link.
Use
Add New / Edit Linked Library
to define the parameters of the linked library.
The window contains two panes, a library pane and a parameter pane. The settings in the
parameter pane are functionally grouped.This table describes the fields in the
Add New / Edit Linked Library
window.Name | Field Type | Description |
|---|---|---|
Select the library you want to link to: | ||
Filter | Text Entry | Apply a filter to find the desired selected library object. |
Connect to Database | Button | Connect to a different database to access additional libraries. |
Libraries in this ACD file | List | Displays selected library objects in the same ACD as the chosen object. Click to select a library object. |
Server ***** | List | Displays selected library objects from other databases or locations. Click to select a library object. |
01 Link Details | ||
Link Name | Text Entry | Mandatory field. Enter the name of the link to be displayed. |
Mandatory | Dropdown menu | True/False option. Set this field to True if the linked library must be resolved before creating, updating, or importing an object. |
Include Condition | Expression | Specifies the expression used to determine whether a linked library is included in Application Code Manager . If the expression is True, the library is included. If the expression is False, the library is not included.Selecting the ellipsis button (...) opens the Expression Builder to write, validate, and test the expression.Only editable when Mandatory is set to False .Default value is Always . |
02 Library Details | ||
Catalog Number | Text Entry | Editable field that displays the catalog number of the selected library object.
The field auto-populates when a library object is selected. Use an underscore (_) as a wildcard for a single character, or a percentage sign
(%) as a wildcard for multiple characters. |
Family | Text Entry | Editable field that displays the family of the selected library object. The field
auto-populates when a value is assigned in the selected library object. Use an underscore (_) as a wildcard for a single character, or a percentage sign
(%) as a wildcard for multiple characters. |
Solution | Text Entry | Editable field that displays the solution of the selected library. The field
auto-populates when a value is assigned in the selected library object. Use an underscore (_) as a wildcard for a single character, or a percentage sign
(%) as a wildcard for multiple characters. |
Library Type | Text Entry | Editable field that displays the library type of the selected library. The field
auto-populates when a value is assigned in the selected library object. Use an underscore (_) as a wildcard for a single character, or a percentage sign
(%) as a wildcard for multiple characters. |
Category | Text Entry | Editable field that displays the category of the selected library. The field
auto-populates when a value is assigned in the selected library object. Use an underscore (_) as a wildcard for a single character, or a percentage sign
(%) as a wildcard for multiple characters. |
Revision | Auto-populate | A rule that defines what version of a library can be linked to. Enter a number if the library version must exactly match, or use the greater than, less than, and equal to signs to specify version numbers greater than, less than or equal to the number specified. For example, >=2 requires that the linked library version be equal to 2 or greater. |
03 Instance Details | ||
Instance Name | Text Entry | Enter an instance name for the linked library. |
Instance Description | Text Entry | Enter a description of the instance. |
Provide Feedback