Edit Alarm

How do I open Edit Alarm?
  1. In
    Library Objects
    , select a controller or local tag that has an alarm.
  2. In the decorator panel, select
    Alarms
    .
  3. Double-click an alarm in the list, edit the properties, then select
    OK
    .
Use
Edit Alarm
to apply decorations to a tag-based alarm condition. Properties that can be edited appear black. Properties that cannot be edited appear gray.
Click the ellipsis button
(...)
next to a property to open the Expression Builder or Substitution Builder for the property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal